Sealing Solutions for Tractors

Tractor_Breakout graphic_1500X800_01
Tractor_Breakout graphic_1500X800_01
Power Train
Power_Train

The power train is formed of the tractor’s engine, which generates power and delivers it to the drivetrain. Engines can have a variety of configurations and sealing solutions are designed to meet the unique requirements of each application. Rotary seals keep oil and grease within the system, while static seals and custom-molded parts prevent ingress of dirt and debris. Drivetrain components perform a vital function, transferring power from the engine to the wheels. Heavy-duty rotary seals, engineered-molded parts and high-performance static seals, keep the tractor operating efficiently. They prevent contamination by mud, dirt and water, protecting components from abrasion and keeping lubricants inside the system.

Cylinders & Actuators
CA

Within hydraulic and pneumatic systems, cylinders and actuators play a critical part. It’s important that sealing systems within them help achieve maximum performance, over a long operating cycle without leakage.

Learn more about hydraulic cylinder sealing

Valves & Pumps
VP

Pumps are in place to generate flow in hydraulic systems, which is then directed and controlled by valves. The resulting force operates the hydraulic components within the tractor itself, as well as any cylinders on the attachments.

To maximize efficiency for the operator, valves and pumps must operate precisely. External media needs to be excluded and time between planned maintenance extended.

Central Tire Inflation System
Tires

Central Tire Inflation Systems (CTIS) are integrated pressure control systems that allow operators to inflate or deflate tire pressures directly from the cabin of the tractor, with a touch of a button.

The right pressure, according to machine configuration and application, boosts the performance of tires, increasing traction, reducing slippage and rolling resistance, with consequently higher productivity during daily operation, both in the field and on the road.

The Turcon® Roto L seal is engineered to extend the lifetime of Central Tire Inflation Systems by lowering friction. Uniquely, it only seals when sealing is required. This reduces friction to lower fuel consumption and there by conserves energy. As seal wear only occurs when pressure is activated, seal lifetime is four times longer than a standard seal.

Fitted successfully on a number of CTIS, Turcon® Roto L seal is also at the heart of the Trelleborg Wheel System market-leading CTIS+.

Implements & Attachments
Attachments

The implements and attachments on tractors enable them to perform a wide range of functions, from mowing fields and lifting or moving material to sowing seeds, spreading fertilizer and digging holes.

Given the proximity these attachments have to the ground, static and mechanical face seals are vital in keeping dirt and contamination out of the system. Linear and rotary seals allow for the smooth and quiet operation of the hydraulic equipment while preventing leakage into the environment.