Turcon® fillers outperform nanoparticles

Turcon® fillers outperform nanoparticles

Turcon® fillers outperform nanoparticles

Despite the buzz, nano is not always best: Trelleborg Sealing Solutions proves through research that the traditional fillers used in the majority of its Turcon® polytetrafluoroethylene-based sealing materials as additives to improve wear reduction outperform nanoparticles as additives.

Current industry buzz is all about the enhancement of seal performance by using nanoparticles as fillers for polytetrafluoroethylene-based sealing materials. Responding to this, Trelleborg Sealing Solutions researched and compared the wear reducing ability of its traditional Turcon® additives to nanoparticles as additives. In these tests the optimized Turcon® additives outperformed the nanoparticles.

Image is of manufacturing of a seal from Turcon® material

“Despite the results showing that our traditional additives outperform nanoparticles, Trelleborg Sealing Solutions will continue to work on sealing nanotechnology,” says Thomas Larsen, who headed up the test program at Trelleborg Sealing Solutions. “Our Turcon® compounds are optimized for service conditions using traditional fillers and are generally difficult to beat. Even so, we will continue to investigate if improvements can be made using nanoparticles.”

Nanoparticle-filled materials did not outperform the wear resistance of Turcon® T05

Trelleborg Sealing Solutions tested PTFE filled with the following nanoparticles: carbon nanotubes (MWCNT), alpha Aluminum Oxide (Al2O3, alpha), beta Aluminum Oxide (Al2O3, beta), Tin Oxide (SnO2), Copper Oxide (CuO), Zinc Oxide (ZnO) and Iron Oxide (Fe2O3) in all cases at 1wt%. Performance was compared to both virgin PTFE and Turcon® T05.

The results demonstrate that different types of nanoparticles have different effects on the wear resistance of PTFE, going from virtually no effect to wear reductions beyond a factor of 50. For some nanoparticles performance was dependent on whether systems were running dry or lubricated. For instance, MWCNT performed very well when dry-running but poor in lubricated conditions while others, such as Al2O3 alpha, gave good overall performance.

None of the nanoparticle filled materials though were capable of out-performing the wear resistance of Turcon® T05, dry-running or lubricated.

Background information:

Virgin polytetrafluoroethylene (PTFE) has very low wear resistance and fillers are added to PTFE to increase its wear resistance in dynamic sealing applications. Nanoparticles, which have at least one dimension in the size range of one to 100 nanometers, offer an alternative to traditional fillers. These are currently receiving much attention as fillers for polymers and are promoted as improving mechanical and tribological properties at a low degree of fill as well as reducing the risk of abrasive action against mating counter surfaces.

Click here:

To find out more about our proprietary materials