Trelleborg Keeps Robots on the Move
Trelleborg Sealing Solutions has worked with leading robotic equipment manufacturers since the first inception of the technology back in the 1960s. Since then, the company has become one of the leading suppliers of sealing solutions for the servomechanism, hydraulic and pneumatic systems that power the movement of robots. To illustrate its capabilities, Trelleborg Sealing Solutions is launching a video and augmented reality brochure.
These systems, with complex configurations of seals, are fundamental to the function of robotic equipment. Solutions are required to operate 24-7 with the minimum of downtime, either planned or unplanned. Specific sealing solutions are required that demonstrate outstanding friction capabilities to extend seal life, minimize wear and facilitate smooth and constant movement.
Yoichi Higuchi, who heads up the Robotics lead group at Trelleborg Sealing Solutions, says: “Robots are revolutionizing the way that our products are manufactured, how we look after our homes and procedures in hospitals, for instance. They are becoming critical to our everyday lives and the applications for high-tech appliances are increasing exponentially.
“The robotics market is expected to boom. According to Transparency Market Research the global market is likely to see growth of around 17% to reach revenues of 147 Billion by 2025. When you consider that every robot that has moving ‘arms’ needs a servomechanism, hydraulic or pneumatic system to control them, requirements for seals are going to be huge and continually become ever more challenging.
“In addition to increasing volume demands, there is a need for maximized performance. And ensuring this is becoming even tougher for component suppliers as robots become more sophisticated, size-optimized, faster, stronger and smarter.”
Trelleborg Sealing Solutions supplies seals to numerous types of robots, including robots for industrial, medical, construction, disaster recovery, probe, surveillance, household, entertainment, drone and personal mobility applications. The video and brochure on robotics from Trelleborg Sealing Solutions explores a variety of typical robot applications and proven sealing solutions.
Go to the Video