Trelleborg Sealing Solutions Showcases Subsea Capabilities

Trelleborg

Trelleborg Sealing Solutions Showcases Subsea Capabilities

The global developer and manufacturer of sealing and bearing products will showcase its range of innovative products, which are aiding deep sea oil and gas harvesting, at the upcoming events:

  • Deep Offshore Technology International at the Aberdeen Exhibition and Conference Centre, October 14-16, at stand D17
  • Element Oilfield Engineering with Polymers at the Millennium Gloucester Hotel, London, October 21-23, 2014 at stand 01

David Brown, who heads up the global offshore oil and gas segment for Trelleborg Sealing Solutions, said: “Our attendance at these two UK-based events is a demonstration of Trelleborg’s ‘global reach, local presence’ commitment.”

Products on show at the conferences will include the market-leading sealing materials Isolast® J9513 and J8325. Isolast® J9513 is a specially developed perfluoroelastomer (FFKM) that is fully compliant with NORSOK M-710 and offers high and low temperature capability, from -4° F to +464° F (-20°C to +240°C). Isolast® J8325 perfluoroelastomer provides unrivalled high temperature performance with a continuous maximum operating temperature of +617°F (+325°C).