ISO Fits and Tolerances - new iPhone app

Trelleborg

ISO Fits and Tolerances - new iPhone app

“ISO Fits & Tolerances” is intuitive and very easy to use. Upon entering the nominal diameter needed, users simply select the tolerance classes for bore and shaft. The app then provides the complete ISO fits definition with all relevant values including the type of fit. Tolerances are shown for the most commonly used ISO tolerance classes, and convenient graphs illustrate these classes by bore and shaft.

The first of many apps to come

“This is the first app from Trelleborg Sealing Solutions, with several more in the works,” says Wolfgang Heinrich, Website Specialist for Trelleborg Sealing Solutions. “We are always looking for ways to make our customers’ working lives easier, and with the workforce becoming more mobile every day, we need to provide tools that can be used on the go.”
Also included with the app is one-touch access to the automatically updated library of Trelleborg Sealing Solutions films and animations on YouTube. For more information, just click ‘Contact’ and you can choose to email or be connected to the Trelleborg Sealing Solutions website.