Bacteria Busters - Hygienic design

Bacteria Busters - Hygienic design

Bacteria Busters - Hygienic design

Gaskets, seals and rough pipe surfaces are potential bacteria havens and hygienic challenges for the food and processing industry. The solution? Hygienic design.

Jürgen Hofmann unlocks a glass cabinet. “Look at this,” he says - it is a length of stainless steel piping, which has a short branch at ninety degrees with a bolted-on cover. “There used to be a sensor in here or a similar device, but it was removed and the tube was blocked off. This means that cleaning liquid cannot enter this dead end and the finish here is so coarse that it is easier for the bacteria to adhere to the surface.”

Design of machines for hygiene-critical operations should facilitate easy and efficient cleaning

This is what Jürgen Hofmann is working to solve. Cleanability is his watchword. He wants the design of machines involved in hygiene-critical operations to facilitate easy and efficient cleaning. Hoffman is about to take over a project run by the Fraunhofer Institute for Process Engineering and Packaging in Germany. It comprises an Internet portal called hygienicprocessing. com, which will be a complete information source with regard to hygienic design, with tips, links, a database of literature and a network of experts.

Hofmann is one of the experts involved in this. For the past nine years, he has been teaching as an academic assistant with the Department of Process Engineering at the Technical University of Munich’s Weihenstephan campus, which specializes in all food-related matters.

Picture shows Jürgen Hofmann, an academic assistant with the Department of Process Engineering at the Technical University of Munich’s Weihenstephan campus

There should be no gaps, holes, grooves or “dead areas” that cannot be cleaned

“Hygienic design is relevant in all areas where it is important to keep equipment clean. This includes pharmaceuticals and cosmetics, and even paint,” he says.

In a way, the aim is simple - cleaning is carried out with liquids. These must be able to flow smoothly through all the piping, valves, taps and pumps of a machine. Hofmann’s job is to ensure that there are no gaps, holes, grooves or “dead areas” that the liquid cannot reach. This requires smooth surfaces, curves that direct liquids in the right direction, and seals and gaskets that fit perfectly.

“In the milk industry, it was standard for seals to be set back from the inner surface of the pipes,” says Hoffman. “This created a gap where microorganisms could flourish. The problem is that much effort is needed to clean this kind of equipment. For example, it is necessary to leave cleaning liquids in the pipes for a long time. Such pipes are still used today, but we have helped to design a version where the seal and the inner surface are flush,” explains Hofmann. However, according to Hofmann, it is too often the case that investment decisions are made separately.

Hygienic design within dairy products processing systems is critical

“There is one budget for investment, and another for maintenance, but you can probably save between 25 and 50 percent over the lifetime of the equipment by using hygienic design - particularly if there is a case of contamination, which can involve colossal costs.”

Not all food products are equally sensitive. For example, beer is less critical than dairy products, because alcohol kills pathogenic bacteria (which makes alcohol-free beer a bigger challenge). The contamination that may be found in beer makes it taste bad, but it is not life threatening. In dairy products, contamination can be more serious and cleaning is crucial. Moreover, some food trends, such as the move away from artificial preservatives, have made hygiene increasingly important.

Trelleborg is a sponsoring member of university testing center that conducts EHEDG tests

For Hofmann, it does not matter what the machinery is processing, the cleaning substance must enter all areas and do its job. The university has a testing center that conducts a cleanability test developed for the European Hygienic Engineering & Design Group (EHEDG). Trelleborg is a sponsoring member of this. The center runs a standardized contaminant through the part to be tested and through a reference pipe. A standardized cleaning process is subsequently performed using 1-percent alkaline detergent. Following this, Agar is used as a culture medium to detect how much contamination remains.

“I enjoy this work, because we can really make a difference,” says Hofmann. “We can influence processes and initiate trends. It’s wonderful when a company designs a new machine using concepts that we have developed.”

Picture shows Turcon® Variseal® Ultra-Clean™

Seal development based on Hoffman’s hygienic design principles

Trelleborg Sealing Solutions work closely with the University of Munich’s Department of Process Engineering and have focused research on sealing designs to meet Hofmann’s hygienic principles.

“We can recommend the optimum seal configurations for food, beverage and pharmaceutical processing,” says Burkhard Ledig, Technical Manager CPI Development Europe. “As an example of developments in this field is the recently launched Turcon® Variseal® Ultra-Clean™.”

Turcon® Variseal® Ultra-Clean™ is the optimum seal for hygienic designs

Variseal® is ideal for use in processing systems as it is compatible with virtually all chemical media, has superior wear resistance, unrivalled friction characteristics and can withstand extreme operating temperatures. PTFE, though, has no elasticity. This means that Turcon® Variseal® needs a spring fitted into the seal profile to energize it. The open spring created an area of dead space where bacteria could potentially be caught.

“We therefore focused on an alternative”, continues Ledig. “The resulting Turcon Variseal Ultra-Clean is unique. The spring required to activate the seal is fully enclosed within a Turcon case. This for manufacturers of food, beverage and pharmaceutical products ensures there is no dead space within the seal, guaranteeing that bacteria cannot accumulate, avoiding the risk of contamination.”

A pub as a classroom

The Department of Process Engineering must be the only Department in the world to have a pub as a classroom. Charly’s Pils Pub (named after the professor, Karl Sommer) is at the leading edge of the brewing industry in terms of hygiene, although it may be lacking as regards pub atmosphere. The bar is equipped with a wide range of taps so that brewery representatives and bar owners can learn which taps are best for which beers. In addition, they can view the latest in cleaning technology.

For more information on sealing in food and beverage applications download brochure

Click here for news on Turcon® Variseal® Ultra-Clean™