Personal tools
Namespaces
Variants
Actions
Navigation
Language

Squeeze

From Sealing Technology & Engineering Glossary
Jump to: navigation, search


3 4 5 A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
Name Squeeze
Definition Compression of the cross-section of an O-ring that causes deformation in the ring, creating an effective barrier to block the passage of the fluid between the mating surfaces; the direction of squeeze in static O-ring seals is both radial and axial, while the direction of squeeze in dynamic seals, due to their installation and movement, is almost only radial.
Comments / Questions