Meine Werkzeuge
Namensräume
Varianten
Navigation
Sprache

Flatness

Aus Sealing Technology & Engineering Glossary
Wechseln zu: Navigation, Suche


3 4 5 A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
Name Flatness
Definition Flatness is a measure of a harder gasket's ability to conform to a flat horizontal surface. Maximum deviation from that surface is the degree to which the sheet is out of flat. OR measure of the amount of deviation in height or thickness of a surface when placed on a plane.
Comments / Questions