Personal tools
Namespaces
Variants
Actions
Navigation
Language

Off or Uneven Register

From Sealing Technology & Engineering Glossary
Jump to: navigation, search


3 4 5 A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
Name Off or Uneven Register
Definition See Offset. Center of the shaft and the center of the housing or bore not being aligned within an acceptable tolerance of no more than 0.010 inch (0.25 mm); usually measured without the shaft moving. See also Offset and Shaft-To-Bore Misalignment (STBM).
Comments / Questions