Personal tools
Namespaces
Variants
Actions
Navigation
Language

Natural Rubber

From Sealing Technology & Engineering Glossary
Jump to: navigation, search


3 4 5 A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
Name Natural Rubber
Definition Also called India Rubber or gum rubber or caoutchouc, an elastomer obtained from the latex sap of trees, particularly of the genera Hevea and Ficus; latex is a milky colloid with the organic compound polyisoprene, an elastic polymer, as its main ingredient. Latex must be refined and vulcanized before it can be used commercially.
Comments / Questions