Personal tools
Namespaces
Variants
Actions
Navigation
Language

DSC

From Sealing Technology & Engineering Glossary
Jump to: navigation, search


3 4 5 A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
Name DSC
Definition Differential Scanning Calorimetry. It is an analysis in which energy input is measured as a function of temperature. It allows to characterize a material's behavior such as: process history, extend of cure, thermal conductivity, glass transition and other material properties.
Comments / Questions