Personal tools
Namespaces
Variants
Actions
Navigation
Language

AA

From Sealing Technology & Engineering Glossary
Jump to: navigation, search


3 4 5 A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
Name AA
Definition Mathematical term used to measure the sum of a series of numbers divided by the number of terms in the series. E.g., AA of the following number: 6, 12, 4, and 15 is (6+12+4+15)/4 = 9.25. AA is sometimes used in surface finish literature where it has the s.
Comments / Questions