E-Catalog
Check out our NEW and IMPROVED Electronic Catalog where you can search for seals by item number, properties or approvals. Submit a request for quotation online.
Go
International WorkBoat Show- Press Kit
29.11.2011
Release #1: Trelleborg Sealing Solutions Goes Mobile
With the global explosion of smartphone devices, Trelleborg Sealing Solutions has developed a portfolio of handy mobile applications and online tools to make seal specification that little bit easier. Among these are two apps for the iPhone and iPod Touch: ‘ISO Fits & Tolerances‘ and ‘Unit and Hardness Converter.‘
The ‘ISO Fits & Tolerances’ app is intuitive and very easy to use. Upon entering the nominal diameter needed, users simply select the tolerance classes for bore and shaft. The app then provides the complete ISO fits definition, based on the ISO 286 System, with all relevant values including the type of fit. ‘Unit and Hardness Converter’ is used to convert frequently used units and commonly used currencies, as well as popular hardness scales. It converts frequently-used units and currencies in an efficient and convenient way, as well as popular hardness scales for various material types based on ISO and ASTM standards.
“These two apps are just the beginning,“ says Wolfgang Heinrich, Website Specialist for Trelleborg Sealing Solutions. “We are always looking for ways to make our customers’ working lives easier, and with the workforce becoming more mobile every day, we’ll continue to provide tools that can be used on the go. Look for several more apps from us in the near future.”
The Trelleborg Sealing Solutions range of easy-to-use online tools include the Sealing Solutions Configuator, Material Search and Chemical Compatibility Check, along with its well-established‚ O-Ring Calculator, Electronic Catalog and the versatile CAD Service. In addition, engineers can keep up-to-date with the latest news and updates from the across the Trelleborg Group with ‘Trelleborg Gateway,’ the app for iPhone and Android that provides quick access to product and contact information and includes an interactive rubber type selector and polymer glossary for engineers.
All Trelleborg applications are entirely free-of-charge and also include one-touch access to the automatically updated library of Trelleborg Sealing Solutions films and animations on YouTube. To find ‘ISO Fits & Tolerances‘ and ‘Unit and Hardness Converter,‘ search for ‘Trelleborg’ in the Apple App Store or in iTunes. ‘Trelleborg Gateway’ can be found in the Apple App Store, in iTunes or on the Android Market using the same search term. Online tools are available at www.tss.trelleborg.com/us.
Latest news
Print Version
To the top